Analog Devices' LT8390 60V Buck-Boost Controller Now at Mouser for Auto, Industrial and Battery Systems
March 7, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the LT8390 synchronous buck-boost DC/DC controller from Linear Technology, now a part of Analog Devices, Inc. The LT8390 controller offers a 4 V - 60 V input voltage range and 0 V - 60 V output voltage range, making it ideal for voltage regulator, battery, and supercapacitor charger applications in automotive, industrial, telecom, and battery-powered systems.
The LT8390 DC/DC controller, available from Mouser Electronics, can regulate output voltage and input or output current from input voltages above, below, and equal to the output voltage. The device's four-switch buck-boost controller, combined with four external N-channel MOSFETs, can deliver from 10 W to over 400 W of power with efficiencies up to 98 percent.
The LT8390 uses a proprietary peak-buck, peak-boost current mode control scheme which uses a single inductor current-sense resistor to provide a seamless transition between buck, boost and buck-boost regions. The device delivers output voltage with ±1.5-percent accuracy, and its output current accuracy of ±3 percent ensures accurate constant current regulation. The LT8390 can be programmed to use a fixed switching frequency between 150 kHz and 650 kHz with synchronization, or it can utilize internal spread spectrum operation for lower electromagnetic interference (EMI). Additional features include an input or output current monitor, power good flag, integrated bootstrap diodes, and short-circuit protection with fault reporting.
The LT8390 controller is available in either a 28-lead QFN or thermally enhanced 28-lead TSSOP package to provide a very compact solution footprint.
To learn more, visit www.mouser.com/adi-lt8390-buck-boost-controllers.
For more information on power electronics, visit Mouser's Power Management Technologies site at www.mouser.com/applications/power-management-technology.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 22 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Analog Devices, Inc.
Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com