Now at Mouser: Maxim's MAX14906 Industrial Digital I/O with Per-Channel Configurability
June 18, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MAX14906 industrial digital output/digital input (digital I/O) from Maxim Integrated.
The Maxim MAX14906 is an IEC 61131-2 compliant, high-speed, four-channel industrial digital I/O can be configured on a per-channel basis as a high-side switch, push-pull driver, or a Type 1 and 3, or Type 2 digital input. The Maxim MAX14906 is specified for operation with a supply voltage up to 40 V and is tolerant of transients up to 65 V. The high-side switch current limiting is settable from 130 mA to 1.2 A with the option of double-load inrush current. The typical high-side driver on-resistance is 120 mΩ at 25 degrees Celsius ambient temperature. The optional push-pull operation allows high-speed driving of cables and fast discharge of load capacitance. For digital input operation, current sinks for 2.3 mA (Type 1 and 3) or 7 mA (Type 2) are provided.
The MAX14906 device is supported by the Maxim MAX14906EVKIT evaluation kit, which monitors the MAX14906 diagnostic information, including open-wire condition, state of the output channels, multiple undervoltage alarms, global and per-channel overtemperature alarms, and multiple fault alarms.
Applications for the MAX14906 include robotics, motor control, and PLC systems.
For more information, visit https://www.mouser.com/new/maxim-integrated/maxim-max14906-digital-output-digital-input/.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 800 manufacturers. Mouser offers 27 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 1 million sq. ft. state-of-the-art facilities south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com