Mouser Now Offering Texas Instruments’ AMC1301 Reinforced Isolated Amplifier

Annuncio di nuovi prodotti

Mouser Now Offering Texas Instruments’ AMC1301 Reinforced Isolated Amplifier

June 30, 2016 - Mouser Electronics, Inc. is now offering the AMC1301 reinforced isolated amplifier from Texas Instruments (TI). The AMC1301 is the industry's first reinforced isolated amplifier to withstand isolation working breakdown voltage of 1,000 VRMS for a minimum insulation barrier lifetime of 40 years.

TI's AMC1301 isolated amplifier, now available from Mouser Electronics, is a highly reliable isolated amplifier with lower power consumption, higher DC accuracy, and improved overall power efficiency compared to similar devices. The amplifier features a low offset drift of 3µV/C over a wide temperature range of -40 to +125 degrees Celsius. The AMC1301 provides 65 percent less high-side-supply current and 45 percent less low-side-supply current than similar devices, improving overall power efficiency, simplifying power supply design, and reducing thermal drift issues for a more efficient system design and improved performance. The amplifier offers high precision with a maximum non-linearity of 0.03 percent and very low gain drift of 50 ppm/degree Celsius.

Mouser is also stocking the TI AMC1301EVM, a full-featured evaluation board for the AMC1301. The AMC1301EVM evaluation module includes four screw terminals for easy access to the amplifier's analog inputs and outputs, and features a fixed gain of 8.2 and ±250-mV input voltage range optimized for current measurement using shunt resistors. The AMC1301EVM provides a reference solution for measuring isolated current using a shunt resistor and the AMC130 amplifier, delivering a highly accurate solution for shunt-based current sensing in high-voltage applications such as industrial motor drives, solar inverters, battery management systems, and uninterruptible power supplies.

To learn more about the TI AMC1301 amplifier and evaluation module, visit http://www.mouser.com/new/Texas-Instruments/ti-amc1301-amplifier/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

In qualità di distributore autorizzato, Mouser Electronics offre la più vasta offerta al mondo di nuovi semiconduttori e componenti elettronici a magazzino e pronti per la spedizione. I clienti di Mouser hanno la certezza di poter contare su prodotti 100% originali, certificati e completamente tracciabili per ciascun produttore. Il sito di Mouser Electronics ospita un'ampia libreria di risorse tecniche per aiutare i suoi clienti a velocizzare i tempi di progettazione. Tra queste, il Centro Risorse Tecniche, include schede tecniche, progetti di riferimento specifici per produttore, note applicative, indicazioni tecniche di progettazione, strumenti di progettazione e molte altre informazioni utili.

Informazioni su Mouser

2026 - Mouser è uno dei principali distributori autorizzati di componenti elettronici e prodotti per l'automazione industriale. Con oltre 6,8 milioni di prodotti di più di 1.200 produttori, offriamo la più ampia selezione di prodotti disponibili a magazzino. La nostra divisione di componenti elettronici affianca ingegneri progettisti e responsabili acquisti offrendo le ultime novità di prodotto nei settori dei semiconduttori, dei componenti passivi, dell'interconnessione e delle tecnologie elettroniche correlate. La nostra divisione di automazione industriale supporta le aziende a progettare, realizzare e mantenere le proprie apparecchiature e attività produttive, offrendo soluzioni all'avanguardia per sensori, pannelli, PLC e sistemi di controllo motore, disponibili a magazzino per la spedizione immediata.

Mouser offre un servizio clienti di eccellenza tramite 28 sedi distribuite in tutto il mondo, con assistenza nella lingua locale e supporto nelle valute e nei fusi orari locali. Ogni giorno spediamo prodotti a più di 650.000 clienti in 223 paesi e territori dai nostri modernissimi centri di distribuzione, con una superficie complessiva di oltre 140.000 metri quadrati, situati nell'area metropolitana di Dallas, Texas. Per ulteriori informazioni, visitare https://www.mouser.com.

Informazioni su Texas Instruments

2026 - Texas Instruments Incorporated è una società globale di semiconduttori che progetta, produce e commercializza chip analogici e per l'elaborazione integrata destinati a mercati quali quello industriale, automobilistico, dell'elettronica di consumo, dei sistemi aziendali e delle apparecchiature di comunicazione. L'obiettivo principale di Texas Instruments è creare un mondo migliore rendendo l'elettronica più accessibile grazie ai semiconduttori. Questa passione è viva ancora oggi, poiché ogni generazione di innovazione si basa sulla precedente per rendere la tecnologia della società più affidabile, più conveniente e a basso consumo energetico, rendendo possibile che semiconduttori entrino nell'elettronica ovunque.

Marchi registrati

Mouser e Mouser Electronics sono marchi registrati di Mouser Electronics, Inc. Altri prodotti, loghi e nomi di società qui citati, possono essere marchi commerciali dei rispettivi proprietari.

Per maggiori informazioni, contattare:
Kevin Hess, Mouser
Vicepresidente senior del marketing
+1 (817) 804-3833
Per richieste stampa contattare:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764