Now at Mouser: STMicroelectronics’s STWLC33 Inductive Power Receiver Delivers 15W Qi and AirFuel Wireless Charging

Annuncio di nuovi prodotti

Now at Mouser: STMicroelectronics’s STWLC33 Inductive Power Receiver Delivers 15W Qi and AirFuel Wir

February 5, 2018 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader that empowers innovation, is now stocking the STWLC33 inductive wireless power receiver from STMicroelectronics (ST). One of ST's Wireless Power Transfer solutions, the STWLC33 is an integrated, multi-mode wireless power-receiver solution optimized for portable high-speed chargeable applications up to 15W. The dual-mode receiver operates with both the Wireless Power Consortium's (WPC) Qi 1.2 and PMA-SR1 AirFuel inductive wireless standard communication protocols, enabling it to quickly start charging mobile devices regardless of protocol.

The ST STWLC33 inductive wireless power receiver, available from Mouser Electronics, greatly simplifies the implementation of dual-function handheld devices and provides an improved user experience, faster wireless charging, and outstanding total system efficiency over other solutions. The STWLC33 is also the only 15W receiver from ST that is capable of acting like a 3W transmitter, using the same coil to provide power to another receiver. Users can charge one device wirelessly while also using that same device to charge another. In addition, the STWLC33 is one of the first wireless receivers on the market capable of providing an output voltage that can charge two-cell lithium-ion batteries.

At the core of the STWLC33 is a 32-bit, 32 MHz Arm® Cortex®-M microcontroller with 32 Kbytes of firmware/ROM memory and 8 Kbytes of RAM. The device delivers a total system efficiency up to 80 percent and low power dissipation through features such as its integrated low impedance synchronous rectifier and low drop-out linear regulator.

The STWLC33 offers patented features that help enhance user experience, including active presence detection to wake the system quickly when a compatible object is presented for charging, and special functionality to enhance the performance of foreign object detection (FOD) to cut power and prevent overheating. Other features include a 32 MHz PWM timer, eight-channel analog-to-digital converter (ADC), and configurable general-purpose inputs and outputs (GPIOs).

ST's STWLC33 inductive wireless power receiver is ideal for very compact wireless applications that include tablets, power banks, phones, medical equipment, and wearable devices. Designers can also combine the STWLC33 receiver with the STWBC-EP wireless charging controller transmitter to complete their high-speed chargeable devices. The STWLC33 is supported by the STEVAL-ISB042V1 evaluation board, which includes STWLC firmware that allows engineers to modify parameters and settings to ensure proper integration of the STWLC33 power receiver into the final application.

To learn more, visit www.mouser.com/stmicroelectronics-stwlc33-power-receiver.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

In qualità di distributore autorizzato, Mouser Electronics offre la più vasta offerta al mondo di nuovi semiconduttori e componenti elettronici a magazzino e pronti per la spedizione. I clienti di Mouser hanno la certezza di poter contare su prodotti 100% originali, certificati e completamente tracciabili per ciascun produttore. Il sito di Mouser Electronics ospita un'ampia libreria di risorse tecniche per aiutare i suoi clienti a velocizzare i tempi di progettazione. Tra queste, il Centro Risorse Tecniche, include schede tecniche, progetti di riferimento specifici per produttore, note applicative, indicazioni tecniche di progettazione, strumenti di progettazione e molte altre informazioni utili.

Informazioni su Mouser

2026 - Mouser è uno dei principali distributori autorizzati di componenti elettronici e prodotti per l'automazione industriale. Con oltre 6,8 milioni di prodotti di più di 1.200 produttori, offriamo la più ampia selezione di prodotti disponibili a magazzino. La nostra divisione di componenti elettronici affianca ingegneri progettisti e responsabili acquisti offrendo le ultime novità di prodotto nei settori dei semiconduttori, dei componenti passivi, dell'interconnessione e delle tecnologie elettroniche correlate. La nostra divisione di automazione industriale supporta le aziende a progettare, realizzare e mantenere le proprie apparecchiature e attività produttive, offrendo soluzioni all'avanguardia per sensori, pannelli, PLC e sistemi di controllo motore, disponibili a magazzino per la spedizione immediata.

Mouser offre un servizio clienti di eccellenza tramite 28 sedi distribuite in tutto il mondo, con assistenza nella lingua locale e supporto nelle valute e nei fusi orari locali. Ogni giorno spediamo prodotti a più di 650.000 clienti in 223 paesi e territori dai nostri modernissimi centri di distribuzione, con una superficie complessiva di oltre 140.000 metri quadrati, situati nell'area metropolitana di Dallas, Texas. Per ulteriori informazioni, visitare https://www.mouser.com.

Informazioni su STMicroelectronics

2026 - STMicroelectronics è un'azienda globale indipendente nel settore dei semiconduttori e un leader nello sviluppo e nella fornitura di soluzioni per semiconduttori su tutta la gamma delle applicazioni di microelettronica. Grazie a un'ineguagliata combinazione tra competenze di sistemi e materiali, forza di produzione, un portafoglio di Proprietà Intellettuali (IP) e partner strategici, STMicroelectronics è all'avanguardia nella tecnologia System-on-Chip (SoC) e i suoi prodotti hanno un ruolo chiave nelle tendenze di convergenza odierne.

Marchi registrati

Mouser e Mouser Electronics sono marchi registrati di Mouser Electronics, Inc. Altri prodotti, loghi e nomi di società qui citati, possono essere marchi commerciali dei rispettivi proprietari.

Per maggiori informazioni, contattare:
Kevin Hess, Mouser
Vicepresidente senior del marketing
+1 (817) 804-3833
Per richieste stampa contattare:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764