Mouser Now Stocking the Renesas RZ/T2L High-Performance Microprocessor, Enabling Real-Time Control for EtherCAT Communication

Annuncio di nuovi prodotti

May 31, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the RZ/T2L high-performance microprocessor with EtherCAT from Renesas Electronics. Optimized for high-speed processing and high-precision real-time control for applications adopting EtherCAT communication protocols, the RZ/T2L inherits the same advanced hardware architecture from Renesas' RZ/T2M MPU. Reducing its overall footprint by up to 50 percent over the RZ/T2M, the RZ/T2L is the perfect cost-effective and scalable alternative for designers and first-time developers looking to enter the rapidly expanding EtherCAT market with a single-chip motor control solution. The device is also ideally suited for applications such as AC servos, inverters, industrial robots, medical equipment, wind turbines and elevators.

The Renesas RZ/T2L microprocessor features an Arm® Cortex®-R52 CPU with a maximum operating frequency of 800 MHz, an Ethernet MAC and a proven 3-port EtherCAT slave controller designed by Beckhoff Automation for Ethernet communication. The MPU's tightly coupled 576 KB of memory is directly connected to the CPU. This design element reduces execution time unpredictability caused by cache memory, enabling reliable, deterministic processing. All RAM on the MPU is also equipped with an error correction code (ECC) function required for industrial applications.

The robust peripheral capabilities of the RZ/T2L include multi-protocol encoder interfaces for angle sensors, Sigma-delta interfaces, 3-phase PWM and 12-bit ADCs. These peripherals are arranged on a dedicated low latency peripheral port (LLPP) bus directly connected to the CPU to achieve fast and accurate real-time control functionality. Other notable features of the RZ/T2L include support for various security functions such as secure boot, secure firmware update, JTAG authentication, unique ID and cryptographic accelerator to reduce the risk of data breach and tampering of user programs. The MPU can also be used as a functional safety microprocessor to meet the growing processing requirements for industrial equipment.

To support the development of the RZ/T2L microprocessor, Renesas offers a companion RZ/T2L Starter Kit+, also available through Mouser Electronics. The MPU and Starter Kit+ utilize Renesas' Flexible Software Package (FSP) and software development environment, which is compatible with other RZ Family MPUs and RA Family MCUs to help designers preserve software assets and reduce development efforts and overall costs.

To learn more about the RZ/T2L high-performance microprocessor, visit https://www.mouser.com/new/renesas/renesas-rz-t2l-mpu/.

To learn more about the RZ-T2L Starter Kit+, visit https://www.mouser.com/new/renesas/renesas-rz-t2l-starter-kit/.

 

In qualità di distributore autorizzato, Mouser Electronics offre la più vasta offerta al mondo di nuovi semiconduttori e componenti elettronici a magazzino e pronti per la spedizione. I clienti di Mouser hanno la certezza di poter contare su prodotti 100% originali, certificati e completamente tracciabili per ciascun produttore. Il sito di Mouser Electronics ospita un'ampia libreria di risorse tecniche per aiutare i suoi clienti a velocizzare i tempi di progettazione. Tra queste, il Centro Risorse Tecniche, include schede tecniche, progetti di riferimento specifici per produttore, note applicative, indicazioni tecniche di progettazione, strumenti di progettazione e molte altre informazioni utili.

Informazioni su Mouser

2026 - Mouser Electronics è un distributore autorizzato di semiconduttori e componenti elettronici specializzato nell'introduzione di nuovi prodotti dei suoi principali produttori partner. Al servizio della comunità globale di progettisti e acquirenti di componenti elettronici, il sito web del distributore globale, mouser.com, è disponibile in diverse lingue e valute e presenta oltre 6,8 milioni di prodotti di più di 1200 marchi di produttori. Mouser offre supporto tecnico con 28 sedi in tutto il mondo per garantire il miglior servizio clienti del settore nella lingua, nella valuta e nel fuso orario locale. L’azienda effettua consegne a livello globale a più di 650.000 clienti dislocati in più di 223 Paesi e territori, dal suo complesso all’avanguardia di 93.000 metri quadrati, situato a sud di Dallas in Texas. Per maggiori informazioni, si prega di visitare https://www.mouser.it.

Informazioni su Renesas Electronics

2026 - Renesas Electronics è un'azienda di semiconduttori con una gamma eccezionale di prodotti leader nel mercato globale. Renesas ha la tecnologia e le capacità per fornire quasi tutto quanto è necessario in un'epoca incentrata sulle esigenze umane, tra cui tecnologie di sicurezza, miniaturizzazione e tecnologie di risparmio energetico, reti e tecnologie di interfaccia. Renesas punta a rimanere un passo avanti e a essere il vero fornitore di soluzioni di chip intelligenti, leader mondiale nel proprio settore.

Marchi registrati

Mouser e Mouser Electronics sono marchi registrati di Mouser Electronics, Inc. Altri prodotti, loghi e nomi di società qui citati, possono essere marchi commerciali dei rispettivi proprietari.

Per maggiori informazioni, contattare:
Kevin Hess, Mouser Electronics
Vicepresidente Senior Marketing
+1 (817) 804-3833
Gli addetti stampa possono contattare:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764